AnsweredAssumed Answered

ADSP BF 548 Enable optimization issue

Question asked by amar26121993 on Jun 13, 2018
Latest reply on Jun 20, 2018 by Jithul_Janardhanan

Dear sir

 

I am working on ADSP BF 548 Evaluation board with VDSP++ compiler ver 5.1.2. Here we are using HOLT chip (HI-6136) for MIL1553B protocol, which we are accessing through SPI interface to read/write registers. This SPI communication with HOLT chip is working fine when “Enable Optimization” is disabled under the Project option->Compile->General. But when “Enable Optimization” is enabled, the SPI communication with HOLT chip is not working.

 

Kindly suggest us, if any other configuration/settings to be done in the code or project settings to overcome this issue at the earliest.

 

Best Regards

Amar TR

Software Engineer 

SLN technologies

Outcomes