AnsweredAssumed Answered

What is the max resistance for MPPC pin in LTC3105?

Question asked by roberto_in on Jun 13, 2018
Latest reply on Jun 27, 2018 by JNoon

I'm using LTC3105 as a trickle charger for a Li-Po battery as shown in the first page of the datasheet, but with a 1W, 5V rated PV panel instead of a single cell one. I'm using a 390k resistor in the MPPC pin because I want the panel to work at 3.9V . Is this correct? When I measure the voltage in the MPPC it varies and usually is around 2.5V and 3V. If the block diagram in the datasheet is correct, there is an internal current source so the voltage should be constant. What is wrong?

Outcomes