AnsweredAssumed Answered

How does the AD9164 generate the 6GHz signal

Question asked by magic_wyc on Jun 12, 2018
Latest reply on Jun 21, 2018 by landsman

hello,I want to use the AD9164 to generate the 6GHz signal.

The DAC is operated in NCO only mode with the 5GHz clock .After configured the related register,the AD9164  operated in NRZ mode and Mix-mode can generate the signal tone sine wave in the first Nyquist zones and the second Nyquist zones(with the FIR85 enabled).

But what could I do operate the AD9164 generate the 6GHz signal and the power is -6dB(showed in datasheet Figure 132).

Outcomes