AnsweredAssumed Answered

Volume Control Depending Switch

Question asked by skhan on Jun 8, 2018
Latest reply on Jun 13, 2018 by skhan

Hallo

 

I am trying to make a set of filters, and i want to switch between the filters depending on the volume control block during run time. So for example initially the volume control stays at 0 dB, then the signal filtered using filter block 1, then the user goes to 5 dB then then we use filter block 2, and if the user goes to -5 dB we change to another filter block. this switching of the filter should happen automatically depending on the change on the volume control. Is it possible to do with Sigma studio blocks? If yes can any one please suggest me how to do it?

 

I am using ADAU 1452 eval board for the test purpose.  

Outcomes