AnsweredAssumed Answered

ADALM-PLUTO serial connection

Question asked by JohnNun on Jun 7, 2018
Latest reply on Aug 14, 2018 by mhennerich

My aim is to talk to ADALM-PLUTO via a Micro Controller using the standard Serial commands.

I have tested all the commands first by using Putty and then a vb.net and everything works fine.

The small amount of data I need is fine at 9600 baud.

The next stage is confusing me. My microcontroller will send Serial TTL.

I have made a test cable and with 2 USB to serial adapters, then 2 terminals working on the windows laptop.

Thats is fine.

When I connect one end of the cable to ADALM-PLUTO via a OTG cable, nothing happens.

Is there a command to tell the firmware to talk via OTG instead of the supplied USB cable?

Do I need to install drivers for the USB to Serial Adapters to work on ADALM-PLUTO. 

I'm new to Linux and ADALM-PLUTO, so any help would be appreciated

Outcomes