AnsweredAssumed Answered

Hi I am working on a design which has  LT6106 current sense amplifier where the VCC is 5V and IN  and IN- is 12V. Device is working now and I want to understand if the internal ESD structure of the IC are specialised enough for this application as when In

Question asked by Shenoy on Jun 7, 2018
Latest reply on Jun 20, 2018 by Shenoy

Hi I am working on a design which has  LT6106 current sense amplifier where the VCC is 5V and IN+ and IN- is 12V. Device is working now and I want to understand if the internal ESD structure of the IC are specialised enough for this application as when Input voltage is higher than the supply voltage.  If not can i have a drop in replacement of that IC which are having such capability as i cant change the design now. opamp

Outcomes