AnsweredAssumed Answered

Can I place parallel uModules spaced out by 20cm on a PCB?

Question asked by maxxtepper on Jun 6, 2018
Latest reply on Jun 17, 2018 by Fil

This question concerns a setup using uModules in parallel with one another. Say I have a square PCB, 20 x 20 cm. I want to place one uModule on the top of the square, and the other close to the bottom of the square. At the absolute bottom is the source for Vin of the uModules. Will these uModules operate with their specified operational characteristics when positioned in such a way, and connected for out-of-phase parallel outputs? (Assume at least one large common plane for ground and for Vout). 

Outcomes