AnsweredAssumed Answered

Dose LTM2893 suit AD7983?

Question asked by QYQ on Jun 5, 2018
Latest reply on Jul 23, 2018 by EricB

Hello everyone

 

I want to use LTM2893 to isolate SPI I/F for AD7983, is AD7983 compatible with the LTM2893?

On the datasheet of LTM2893, It is mentioned LTM2893 is optimized for isolating 1Msps high resolution 18-bit SAR ADCs, but these are only some suited legacy LTC ADCs on datasheet.

Do you have any recommended legacy ADI ADCs which can work well with LTM2893? 

 

Best ragards

 

QI

Outcomes