AnsweredAssumed Answered

Which ADC maps the similar features with "AD9826" but speed should be >10Mhz ???

Question asked by rajesh@sysargus.com on Jun 5, 2018

In one of our project we are using "Complete 16-Bit Imaging Signal Processor 'AD9826'"  .

The maximum Speed of AD9826 is limited to 5Mhz as given in the datasheet.

(fADCCLK = 15 MHz, fCDSCLK1 = fCDSCLK2 = 5 MHz)

Requirement:

In new project we need ADC of similar features with ENHANCED speed.(>5MHz). may be 50MHz 0r comparable

 

Please suggest the relevant ADC part number.

Outcomes