AnsweredAssumed Answered

ADRV9361-Z7035 1CRR

Question asked by wm-wm on Jun 5, 2018
Latest reply on Jun 15, 2018 by CsomI
Hi everyone,
I want to use ADRV9361-Z7035 for a particular application involving a detection of certain bandwidth and then re-transmit the detected peaks .
I have the following questions.
a. For RF spectrum detection and re-transmission I want to develop a customize IP and later integrate with FPGA reference design provided by AD.
For this I had built the reference design by cloning HDL source using Vivado 2017_r1. I need help in this regard that between which blocks I should integrate my customize IP.
b. Later once the VHDL design(customize IP integration) complete , whenever ADRV9361-z7035 is power on and after runnig IIO Oscilloscope I want that it should be calibrate according 
to logic (RX LO should be tune to a particular frequency , Bandwidth should be to particular value etc and same is the case with TX ).
for part b. I need some clarity and guidance that should i need to play around with source code/API provided by AD to configure my adrv9361-z7035 for customize settings
any useful link or documentation over there . kindly share the link 
 Thanks in advance for reply!

Outcomes