AnsweredAssumed Answered

Using LT1619 as high voltage flyback converter

Question asked by avihai on Jun 3, 2018
Latest reply on Jun 5, 2018 by avihai

Hi,

I'd like to use the LT1619 as a flyback converter from 10V to 1200V with Iout<1mA. If Vin is too high, also lower values of Vin are acceptable.

I'm looking for an application note or a reference design to implement it in the simplest possible way.

Efficiency is not an issue.

The reason that I chose the LT1619 for this task is that I want to use a PWM signal as the enable (in the S/S pin), so also other controllers with this capability are possible, but I didn't find any alternatives.

 

Thanks

Outcomes