AnsweredAssumed Answered

Configure HMC T2220 via Ni-VISA etheret

Question asked by gverma Employee on May 31, 2018

 I am trying to connect my Hittite HMC-T2220 microwave signal generator in NiMax as per link mentioned below

Ethernet Instrument Control Tutorial - National Instruments 

I'm getting the error "VISA: (Hex 0xBFFF0011) Insufficient location information or the device or resource is not present in the system."

 

I am connecting HMC via ethernet port on it and a static IP set to 192.168.001.015. I am able to ping this ip from my windows PC which also has a static ip configured and directly connected to hmc t2220 via Ethernet cable.

 

Please suggest some example code for connecting to htc t2220 via c# code using Ethernet interface.

Outcomes