AnsweredAssumed Answered

AD9523-1

Question asked by veena on May 31, 2018
Latest reply on Jul 9, 2018 by lallison

I am using AD9523-1 in my design.  I am giving 125 MHz clock  to the  OSC_IN#  and 50MHz I/P to the REF A .

PD# = '1'

REF_SEL='0'

REF_Test='0'

EEPROM_SEL='0'

STATUS0/SP0='0'

STATUS0/SP1='0'

SYNC# = '1'

W1='0' and W0='0'

 

I have attached the schematic, register dump values  and the image of 125MHz  which i am giving to the OSC_IN# pin. But i am not able to see any output at OUT1 and OUT1#

Attachments

Outcomes