AnsweredAssumed Answered

Transient behavior on first samples of AD7980

Question asked by percy on May 30, 2018
Latest reply on Jun 4, 2018 by RobK

I am using the AD7980 where I sample 512 values, delay for 10ms then start again. To test the ADC I just input a fixed voltage. But what I am finding is that about the first 30 samples exhibit some form of transient behavior (see image). After that the data seems OK. The ADC is being driven using a buffer amp. I did also have a low pass filter before the ADC but temporarily removed it as it didn't seem to alter the result. Does anyone have any suggestions on what could be causing this? Thanks

 

Outcomes