AnsweredAssumed Answered

Error of generateing SDSOC platform of AD9361 on Vivado

Question asked by lijiahao554579@163.com on May 30, 2018
Latest reply on May 31, 2018 by lijiahao554579@163.com

Hey guys,

   Hope all are doing fine.

I need to generate a SDSOC platform project for further work. And i followed the guide on Xilinx SDSoc Targeting Example to finish the generation of a FMCOMMS2 SDSoC Platform on ZC702. I did everything as the generation steps shown, but when it comes to running the script sdsoc_platform/sdsoc_platform.tcl , errors show out as follow:

couldn't read file "D:/SDX_example/hdl-2018_r1/projects/fmcomms2/zc702/sdsoc_platform/projects/scripts/adi_project.tcl": no such file or directory
while executing
"source $ad_hdl_dir/projects/scripts/adi_project.tcl"
(file "./system_project.tcl" line 3)

it seems like a directory of script problem, so i went into the script ./system_project.tcl   and changed the thrid row of it from

source $ad_hdl_dir/projects/scripts/adi_project.tcl

to 

source ../../scripts/adi_project.tcl

But nothing better happened, the TCL showed me another werid error as:

couldn't read file "adi_project.tcl": no such file or directory
while executing
"source adi_project.tcl"
(file "./system_project.tcl" line 3)

Then i did some other modification to the two suspicious script and the generation cannot be finished normally, so i doubt that the giude of the generation is so simple and maybe 

Outcomes