AnsweredAssumed Answered

ADP5091的电阻配置问题

Question asked by Lciendf on May 26, 2018
Latest reply on May 27, 2018 by Kevin.Yao

为了在5091上使用锂电池,我做了如下配置,使得充电电压小于4.2V,放电电压高于2.7V 

Rpg1=6.2M Rpg2=3M        Vpg=3.06V

Rte1=5.6M Rte2=3.3M      Vte=4.08V

Rbk1=6.8M Rbk2=3.0M     Vbk=3.25

Rsd1=6.8M Rsd2=3.9M     Vsd=2.7V

 

但是目前出现了一个问题,当使用超级电容测试实际阈值时,Vin接稳压电源(3.2V),电容电压从mV上升到2.5V。随后电容电压不再升高。无电流流入电容。此时adp5091REGOUT无输出,sys有4V左右的输出

把电压=3.5V时,ADP5109重新给电容充电,并且REGOUT出现输出,请问这是为什么?

另:但是我在端口负载时,电容放电截止并非2.7V,为什么,如何控制放电阈值

Kevin.Yao,如有打扰之处,请多谅解

Outcomes