AnsweredAssumed Answered

Is it safe to power two AD9371 devices from a single ADP5054?

Question asked by RajatRao on May 26, 2018
Latest reply on May 29, 2018 by Jason_Duan

The AD9371 eval board uses an ADP5054 to power the AD9371. The ADP5054 can drive upto 6A on channels 1 and 2. The AD9371 only requires 2.1A, 1.1A in these power domains. So, can a single ADP5054 be used to power two AD9371 devices? Can it handle the surge currents, etc.?

Outcomes