AnsweredAssumed Answered

ADL5391 eval board R1 resistor missing?

Question asked by heresjohnny on May 25, 2018
Latest reply on May 29, 2018 by jdobler

Am I understanding something incorrectly in the datasheet?  It says that R1, a 56.2Ohm resistor is by default on there, but looking at R1, no R1 resistor looks visible, looks like a solder between XM_DC and one pad of R1 and the other pad is soldered to XP_DC, in the same matter that R10 and R9 are 0 ohm resistors to the DC test loops of YP and YM?

 

Is that correct?

Datasheet: http://www.analog.com/media/en/technical-documentation/data-sheets/ADL5391.pdf , pic below

 

No R1 resistor visible, looks like a solder between XM_DC and one pad of R1 and the other pad is soldered to XP_DC?

Outcomes