AnsweredAssumed Answered

Very precise 54V DC power supply

Question asked by SBeron on May 24, 2018
Latest reply on May 31, 2018 by nenger

I need to build a very stable DC power supply with a variable output (51 to 56 VDC) at a very low current output ( 100 mA). But the driff and stability needs to be very less than 5 mV. The circuit will not be operating in very significant temperature changes. Which of the many Linear voltage reference should I be considering for this application?

 

Regards

 

Santiago Beron

Outcomes