AnsweredAssumed Answered

2kHz pulse output using ADuCRF101

Question asked by keli on Dec 19, 2011
Latest reply on Dec 30, 2011 by MMA

Using ADuCRF101, I need generate frequency variable pulse output of 50% duty cycle. The frequency ranges from 0 to 2 kHz. Can any member give me some guide on this? Example code will be highly appreciated!

 

The frequency should be updated per the result of internal arithmetic computation. The update rate is up to a few hundred Hertz. What register shall I use to store the computation result and be used to set the pulse frequency.

Outcomes