AnsweredAssumed Answered

Can't read data from AD5933

Question asked by SepehrM on May 22, 2018
Latest reply on Jul 3, 2018 by SepehrM

Hi, I'm using an AD5933 with ATxmega128A1U through an I2C interface with MCLK=1MHz. Everything seems to be working fine and I have been able to write data onto the slave successfully. The problem is, however, that I still can't read data from it. On the output of the oscilloscope, I expect a 0x90 value with NACK, but I keep getting 0x00 with NACK. I would really appreciate any help with this issue.

P.S.: I have attached my C code, along with screenshots of the output of the oscilloscope and also the schematics of the circuit I'm using.

 

S.M

Outcomes