AnsweredAssumed Answered

LTC4020 and microcontroller ground connections

Question asked by OSM on May 21, 2018
Latest reply on Jun 20, 2018 by WATaylor

Hello,

 

We are working on a project which uses the LTC4020 Multi-Chemistry battery charger. Additionally, the design includes a microcontroller ( NXP KL25Z) to provide additional outputs and communication capabilities.

 

The LTC4020 must be connected to SGND and PGND, and both planes must be connected at a single point to follow the star ground philosophy. In the DC2044A demonstration circuit, this connection is made directly under the IC, so we tried to follow this approach in our PCB.

 

The microcontroller has separate pins for analog and digital grounds (AGND and DGND), so we have a total of four grounds in the design (SGND, PGND, AGND and DGND). I think we can treat SGND and AGND the same, but I am not so sure about what to do with the remaining grounds.

 

In the article "Staying well grounded" from Analog Devices, the author suggests that the analog ground must be used as the return path for the analog and digital circuitry in mixed-signal devices, provided that the return currents from the digital section are not too high. Unfortunately, I do not believe this is the case with the microcontroller .

 

On the one hand we wouldn't like to use the AGND/SGND plane as the return path for the digital circuitry of the microcontroller because the fast switching transients may induce some noise in the analog section, but on the other hand using three different ground planes might not be a good idea.

 

Is using three different ground planes the best approach in this application?

What is the best strategy to connect these three ground planes?

 

 

Thanks in advance.

Outcomes