AnsweredAssumed Answered

Question:  will the ADRF5044 switch function properly using -2.5V instead of -3.3V for Vss?  If degradation occurs, what is the magnitude of the change in insertion loss and IP3?

Question asked by tjjournot@mms on May 21, 2018
Latest reply on May 31, 2018 by tjjournot@mms

will the ADRF5044 switch function within nominal specifications using -2.5V instead of -3.3V for Vss.  If not, what is the magnitude of the change in insertion loss and IP3?

Outcomes