AnsweredAssumed Answered

SigmaStudio 3.5 Export System files Problem

Question asked by rwalborn on Dec 17, 2011
Latest reply on Jan 16, 2012 by BrettG

SigmaStudio 3.5 Build 7 Rev 912 12/6/2011 32 bit runnign on XP SP3

 

AD1940

 

I recently upgraded to 3.5 from 3.4 . Now the system export files have added IC_1 in the date defines

for these sections

 

/* Register Default - CoreReg */
#define R5_IC_1_ADDR_IC_1            0xA52_IC_1
#define R5_IC_1_IC_1_SIZE 2
ADI_REG_TYPE R5_IC_1_IC_1_Default[R5_IC_1_IC_1_SIZE] = {
0x02, 0x00
};

 

#define R0_IC_1_ADDR_IC_1           0xA52_IC_1
#define R0_IC_1_IC_1_SIZE 2
ADI_REG_TYPE R0_IC_1_IC_1_Default[R0_IC_1_IC_1_SIZE] = {
0x00, 0x00
};

 


/* DSP Program Data */
#define PROGRAM_SIZE_IC_1 7680
#define PROGRAM_ADDR_IC_1 1024

 

Anybody else seeing this?

Outcomes