AnsweredAssumed Answered

Why ADAS1000 always Busy

Question asked by duduzhuzi on May 19, 2018
Latest reply on May 25, 2018 by CatherineR

SPI can use. Write the register as Example 4. But the DRDY I/O always high, and the OPSTAT register(0x1F) is 0x0004. Read by the frames mode(0x40), the Frame Header is 0xC0000.  All the Ready bit is 1.Write the register as Example 1. The status is also like Example 1. 

Is there any operation I should do after reset the chip? Why it always be busy?

Thanks!

Outcomes