AnsweredAssumed Answered

About ADXL354 SELF TEST

Question asked by OTI on May 17, 2018
Latest reply on May 17, 2018 by NevadaMark

Let me ask SERUFUSESUTO of dataseet P31, please.

 

(1)Are they able to receive more in-depth material about self test?

 

(2) (1) but when it isn't possible, let me do the following question, please.

    1: The time of a self-test mode changes the distance during a pole of each axis by the obctrostatic power,

      and  measuring?

    2: How many G is the acceleration from which I can get ST1 when making Hi,ST2 Low, considerable?

      0g (offset)?

    3:When doing Hi/Low control of ST2, does X/Y/all Z axes change at the same time?

    4:Is it possible of ST2 to do own dynamic acceleration check including a sine wave?

Outcomes