AnsweredAssumed Answered

AD8362 single end vs differential input @ 100MHz

Question asked by sss on May 16, 2018

Hi all,

 

The data of Single end input is ≥450MHz @ AD8362.

Figure 49. Transfer Function at Various Frequencies when the RF Input is Driven Single-Ended

Figure 51. Transfer Function at Various Frequencies ≥2.7 GHz when the RF Input is Driven Single-Ended

The other data is differential input.


The customer target frequency is 140MHz and 1.5GHz w/single end input.

 

Is following data available ?

AD8362 single end vs differential input @ 100MHz.

For example, It is like include the 100MHz data to Figure 49.

 


Best regards,

sss

Outcomes