AnsweredAssumed Answered

AD-FMCDAQ2-EBZ No-OS Drivers config.h file errors

Question asked by sunnysunny3145 on May 14, 2018
Latest reply on May 16, 2018 by sunnysunny3145

Hello ! I have started working with AD-FMCDAQ2-EBZ board and after successfully building hdl project in Vivado I want to implement No-OS drivers. I follow the AD-FMCDAQ2-EBZ Bare Metal Quick Start Guide on this link 

AD-FMCDAQ2-EBZ Bare Metal Quick Start Guide [Analog Devices Wiki] 

And try to download all the files I need for the reference design. Since I was using the Vivado 2016.4, I decided to follow the branch of 2017_r1. However, after I got all the files mentioned in the link, the SDK builder told me that there is a file named config.h missing. I tried to use the file here:
https://github.com/analogdevicesinc/no-OS/blob/2017_R1/fmcdaq2/config.h

The SDK shows more errors like:
Description Resource Path Location Type
expected declaration specifiers or '...' before string constant config.h /0604_test1/src line 70 C/C++ Problem

and lots of errors on
Description Resource Path Location Type
unknown type name 'int32_t' ad9144.c /0604_test1/src line 48 C/C++ Problem

Here I attached the screenshot on the errors. 

Did I pick the correct config.h file for this project? So appreciate if anyone could help me on it.

Outcomes