AnsweredAssumed Answered

FMC Vadj error code 2?

Question asked by RJBell on May 14, 2018
Latest reply on May 15, 2018 by RJBell

Hi,

I just purchased the EVAL-AD9467 kit with the SDP-H1 controller and the AD9467-FMC-250EBZ board. After following the user guide instructions and installing the software under Windows 7 64BIT, then setting up the hardware I cannot get past the following error:  Type Initializer HadSDPSupport.Hardware exception SDP error 100025: Error setting FMC Adj error code 2.  The SDP-H1 SYS_POWER and BF_POWER LEDs are on.  I have uninstalled and reinstalled the software twice and checked to make sure the device driver is installed. Anyone know where I can go to find more information on this specific error OR can suggest where I might have gone wrong during the set-up? 

 

Thanks

Outcomes