AnsweredAssumed Answered

HMC1063 as vector modulator. DC values on IF?

Question asked by eguerrero on May 14, 2018
Latest reply on Jun 6, 2018 by huangzeyan

I want to use IQ mixer HMC1063 as a vector modulator and want to perform phase shifts using DC inputs on the IF ports. These ports support DC to 3 GHz but no actual DC range is specified in the data sheet other than that an IF port should not sink more than 3 mA. Does anyone know which is this DC range to be used on IF ports? I do not want the device to burn or malfunction.

 

Thanks in advance.

Outcomes