AnsweredAssumed Answered

ZC702 FMCOMMS2/3 Matlab 2017b Missing Board selection

Question asked by ddk on May 14, 2018
Latest reply on May 15, 2018 by ddk

Hi, After updating my HDL-WA-BPS to the current master, options for the ZC702 with FMCOMMS boards do not show up in my HDL-WA Target platform selection ( 1.1 in HDL-WA ).


There are lots of new ones, but none that seem to correspond with the ZC702 and FMCOMMS2/3 configuration.
The closest seems to be for the AD9364 radio with a ZC7020, not the AD9361 with ZC7020 and the HDMI controller ( ZC702 Dev board )

 

I can select the ZC706, and therafter select the  RX path option, but no ZC702.

 

I get the following errors for a few boards ( zed , zc702, zc706 for fmcomms 2 and fmcomms5) in the Matlab command window :

Warning: Invalid plugin "AnalogDevices.fmcomms2.zed.rx_tx.plugin_board" is detected with error message "Undefined variable"AnalogDevices" or class "AnalogDevices.fmcomms2.zed.rx_tx.plugin_board".". 
Warning: Invalid plugin "AnalogDevices.fmcomms2.zc702.rx.plugin_board" is detected with error message "Undefined variable"AnalogDevices" or class "AnalogDevices.fmcomms2.zc702.rx.plugin_board".".
...
Warning: Invalid plugin "AnalogDevices.fmcomms5.zc706.rx_tx.plugin_board" is detected with error message "Undefinedvariable "AnalogDevices" or class "AnalogDevices.fmcomms5.zc706.rx_tx.plugin_board".". 


Git repo ( latest commit : 750189f )

HDL Coder BSP Tools  : Version 1.07        (R2017b)
HDL Coder BSP: Analog Devices Inc  : Version 1.07        (R2017b)

 

 

-Daniel

Outcomes