AnsweredAssumed Answered

Can we modulating Thermoelectric cooler

Question asked by uunhyung on May 14, 2018
Latest reply on May 17, 2018 by ytu

If the ramp signal is applied instead of the square signal PWM which is mainly used to control the TEC, does the TEC change linearly to the ramp signal?

The ramp signal duration I want to use is about 10 ms and the temperature difference between the minimum signal and the maximum signal is 5 ° C.

 

I need help from people who have a lot of knowledge about TEC.

Outcomes