AnsweredAssumed Answered

Trouble finding the "frame clock"

Question asked by QIE1.38*10^-23 on May 10, 2018
Latest reply on Jun 1, 2018 by AdrianC

Hello All,

I'm trying to get the talk to an AD-FMCADC3-3BZ with the AD9625 chip on it. I want it to send the ila data to me as described in the JESD204B protocol. I am unsure about a few things though. I need to know exactly when to change the ~sync pin, how long to hold it, and when to send the SYS-REF signal. I have read the documentation and it says that the ~sync signal needs to be synchronized with the "frame clock". I then look for a definition for the "frame clock" and find nothing. I found the documentation put out by JEDEC and they say it is: "A signal used for sequencing frames or monitoring their alignment. " which is pretty useless. I have a clock which latches in the data from the adc and into the fpga. Lets call it the RXUSRCLK2.This clock is going at about 6.4 ns / tic. Another clock is going 5 ns / tic. Lets call it the system clock. There are other clocks generated by the QPLL and I can always slow one of these down. I am using Xilinix Virtex 7 VC707 to run this thing. I have gotten the SPI to work in both read and write modes so I have access to all the registers. Please let me know if you have dealt with these systems before. Some simulations showing the precise timing of these signals would be sufficient.

Thanks.

Outcomes