AnsweredAssumed Answered

ADF4355-3 OUTPUT POWER AND PHASE NOISE PROBLEM

Question asked by kalupen on May 9, 2018

Sir, I made a custom board of adf 4355-3  for frequency range of 5115-5690MHz. Reference is 122.88MHz from clean signal source.The problem here is the output power is @ 5115MHz is -12dBm.even if i choose +5dBm in R6 register.Does RF output require any change in inductor or capacitor to improve the output level.Please suggest me how to improve the output level and achieve better phase noise.

Outcomes