AnsweredAssumed Answered

About ADL5521

Question asked by Alan_Lu on May 8, 2018

Hello:

    When I use the given peripheral components (2140MHz) on the datasheet to configure the ADL5521 chip, the chip attenuates the input signal about 10dB, does not play the role of amplification, but the current consumption can be observed from the voltage source, and supplied power and the bias resistance are all normal. Besides, the replacement of the same chip is still the same result. Excuse me, what is the cause of this? How can I check out which part of the  chip or which pin has problems? Thanks!

Outcomes