AnsweredAssumed Answered

Is the maximum sample rate 500 MSPS as stated in table 4? Or 1 GSPS as stated in pag.27?

Question asked by ritacp on May 4, 2018
Latest reply on May 4, 2018 by UmeshJ

At pag. 27 of AD9684 datasheet it is stated "The AD9684 can be clocked at 2 GHz with the internal clock divider set to 2." . If this statement is true then the AD9684 is a 1 GHz ADC instead of 500 MSPS. Is this correct?

 

This question was already asked in another way. But as there are some mistakes in the datasheet, still is not clear to me.

Outcomes