AnsweredAssumed Answered

Can I connect and control two ADAU1361 Eval boards at the same time with one PC?  Note they are hard wired to the same I2C address (but on different USB ports)

Question asked by jepporob on May 3, 2018
Latest reply on May 10, 2018 by DaveThib

I have two ADAU1361 EVAL boards that I want to use together in a larger system.  I tried connecting them both today, and configured SigmaStudio to have both boards in my project.  But I could not get audio throughput on both of them at once.  

 

Also, I'm wondering if I can configure these EVMs to power up to a working state (basic audio pass-through), or do they required a PC connected to initialize them to pass signal?

Outcomes