AnsweredAssumed Answered

Difficulties with BF548 SPI Boot

Question asked by Johan@Hannes on Dec 14, 2011
Latest reply on Dec 19, 2011 by Andreas

Hi,

 

i was trying to start an application via SPI and boot from Flash - first bootloader, afterwards application. I've two totaly identical Eval Boards EZK BF 548 Lite. Since there is an EEPROM attached on same SPI interface on one board second boot won't work after reading some bytes from EEPROM before and reseting SPI settings. Defenetly there is a problem with bfrom_SpiBoot() - i would appr. if anyone could give me a wink!

 

On the second board both - boootloader and application - will boot without any difficulties.

 

Common questions:

1) Which setup is used for SPI boot and where one can get information about it? Note: Init file has been included!

 

 

2)

Outcomes