AnsweredAssumed Answered

ICE-1000 does not load the program on custom board (ADSP-SC584)

Question asked by Ismurat on May 3, 2018
Latest reply on May 14, 2018 by Kader.M

Hello

I have the ICE-1000, ADZS-SC584-EZLITE, custom board (ADSP-SC584) and I have the following problem:

The same program works on ADZS-SC584-EZLITE, but does not work on a custom board. While loading, via JTAG, the CCSE writes "Load complete" (image 1). If I disable the option "Run Immediately after load", it turns out as on image 2. The program on the custom board does not work. On the custom board DDR and flash are as on ADZS-SC584-EZLITE.

Attachments

Outcomes