AnsweredAssumed Answered

ADPA7006 Question: What is the specification for VGG1 and Absolute Maximum Ratings on VDD and VGG pins

Question asked by Sakshi on May 3, 2018
Latest reply on May 29, 2018 by jdobler

1. What is the operatng value for VGG pin

2. What are the ratings for for VGG and VDD pins?

3. And what is the IDD expected when the device is operated at 4.8V or 5V? Can I get a VDD vs IDD curve?

Outcomes