AnsweredAssumed Answered

AD9361 min. sampling rate for Rx

Question asked by MarcinPol on May 2, 2018
Latest reply on May 4, 2018 by mhennerich

Hi, 

I was wondering what is a minimum sampling rate (and a minimum analog BW) of the Rx channel. The datasheet says it's <200kHz. Is there an exact minimum instantaneous BW the receiver supports? For example, If I want to receive a signal with 50 kHz BW do I need to oversample the channel with a minimum 200 kHz BW or is it possible to lower the bandwidth of AD9361 Rx below 200 kHz?  

 

Thanks,

Marcin

Outcomes