AnsweredAssumed Answered

What is the max memory size of HSC-ADC-EVALB-xx

Question asked by Yoh on Dec 14, 2011
Latest reply on Dec 16, 2011 by AndyR

Hi,

 

I want to use the FPGA based evauation board to hook up to and ADC board, capture samples and process live (not necessarily real time). To do this I need to be able to capture large sample size (about 10MB). The eval boards as specified only have 32/64 kB of memory on board - but I read in one of the datasheets that this memory is expandable. Does anyone know the maximum size that the memory can be set to? Is the maximum size something that I can preorder so that the eval board comes populated with the right memory size or something that has to be retrofitted with an external memory?

 

Thanks in advance

Yohannes

Outcomes