AnsweredAssumed Answered

Power pins show short with ground for EVAL-AD9959

Question asked by t.sawant1069 on Apr 30, 2018
Latest reply on May 11, 2018 by mcee

We have an evaluation board for AD9959 DDS.  After examining the power supply pins on the board, 2 of them (DVDD and VCC_USB) are showing short with the ground. If I measure the resistance between the pins and ground I get 4.7 ohm, 7 ohm and 60 ohm for DVDD, VCC_USB and DVDD_IO respectively.  I also checked the current drawn by the board after applying a small voltage to the power pins. The current drawn is consistent with the measured resistance. 

Outcomes