AnsweredAssumed Answered

LT8610AC In parallel or in the same board

Question asked by Lucis on Apr 30, 2018
Latest reply on Apr 30, 2018 by EHorsma

Hello,

I'm designing a regulator from 28V to 5 - 5.1 V and I would like to place two LT8610AC. Is there a recommendation/application note on the connection/synchronization of two LT8610AC in the same board? I'm evaluating two options:

- Place two of them sharing the same load;

- Place two of them driving different portions of load at the same nominal VOut.

 

What would you suggest?

 

Thanks in advance.

 

Luca

Outcomes