AnsweredAssumed Answered

LTM4622 INTVcc details

Question asked by davisbm3 on Apr 27, 2018
Latest reply on Apr 27, 2018 by SYoung

I noticed in several of the application examples INTVcc is used to power supporting circuitry (specifically oscillator distribution).

 

1) If I was to use this power for a similar purpose, what is a reasonable current It can provide? (the data sheet implies up to 50mA with the specification for 1.3% line regulation from 0 to 50 mA).

 

2) Is this always on? or is it only on when one of the power supplies is running?

Outcomes