AnsweredAssumed Answered

The Max MIPS

Question asked by fjlasjdfkj322038402 on Apr 27, 2018
Latest reply on May 8, 2018 by Sakthi^vel

Hi,

 

I design a SigmaStudio schematic. Add lots of modules. And I listen to the output sound. NO!

 

Then I delete some modules and listening again. Until the sound is correct. Is this development efficiency too low?

 

When I think it's all right. I found that reading the "readback" module will affect the output sound. So I have to continue to delete some modules. Until the sound is correct.

 

Such a development is a great headache!

 

When the FS is 96K, the application only reach average 120 MIPS. If greater than 120, the sound is wrong.

Are there any better ways and ideas.

 

My target is ADSP-21489, 400MHz

 

Thanks!

Chen

 

Outcomes