AnsweredAssumed Answered

P1dB and IP3 of ADRF5020 @ 40GHz

Question asked by kkADI on Apr 24, 2018

Hi,

 

   In ADRF5020 product datasheet, there is mention of P1dB and IP3 measurement results up to 26 GHz. I understood the part is intended for frequency range 100 MHz to 30 GHz but just wonder if you do have P1dB & IP3 measurement data for RF frequency up to 40 GHz?

 

  Also please advise test conditions (tone spacing, tone input RF power, RFC-RF1 or RFC-RF2 port) of IP3 for ADRF5020.

 

Thank.

Outcomes