AnsweredAssumed Answered

ADF5355 Balun

Question asked by pmico on Apr 19, 2018

Dear Mr/Mrs

 

I need that the ADF5355 generate a frequency range from 60-600MHz with a single-end output.

I am thinking to combine RFOUTA+- with the wideband RF transformer TCM1-63AX+ from Minicircuits.

If I set the current in order to achive +5dBm output power (Bits[D2:D1] in Register 6.)

Would I have 3dB (+8dBm) higher power if I use that RF transfomer?.

 

Thank you very much in advanced.

Best

Pablo 

Outcomes