AnsweredAssumed Answered

Using the ADALM-JTAGUART with Xilinx Vivado/SDK

Question asked by Superluminal on Apr 17, 2018
Latest reply on Apr 17, 2018 by Superluminal

Hi all,

 

I've just received my ADALM-PLUTO and would like to use it to try and use it to build an ADSB Mode-S receiver. The plan is to use the Pluto as a "bare board" and implement my own design, i.e. custom VHDL and C using the Xilinx Vivado/SDK for the on board Zynq. It's an ambitious project, but I'm looking forward to the challenge!

 

I need to fit a JTAG header and was planning to buy the ADALM-JTAGUART, but have two "simple" questions...

 

1. Is this device compatible with Vivado? i.e. will it be recognised or do I have to use it in conjunction with another JTAG programmer?

 

2. Does the device export the on board Pluto UART as a Virtual COM port?

 

Many thanks!

 

Max

Outcomes