AnsweredAssumed Answered

ADA4817 quiescent current during nonlinear operation

Question asked by Yuya on Apr 17, 2018
Latest reply on Apr 18, 2018 by Yuya

Hi,

My customers are considering using ADA 4817.

 

It seems that they want to know quiescent current during nonlinear operation.
Vs: ± 5 V
Gain: × 5
Input: 4 Vp-p

 

#1  When using under the above conditions, does the quiescent current increase from the MAX value (21 mA) of the

      quiescent current of the data sheet(When they use ±5 V Vs)?

 

Best Regards,

Yuya

Outcomes